BaseExplicitOrderBuilder Class |
This is the NXOpen.Gateway.BaseExplicitOrderBuilder for the explicit order |
BookmarkFile Class |
Represents operations which can be done on bookmark files. |
CopyCutBuilder Class |
Represents a NXOpen.Gateway.CopyCutBuilder |
GenericFileNewBuilder Class |
Represents a builder class that performs Generic File New operations. |
IGenericFileNewApplicationBuilder Class |
Represents the class Application Builder. |
ImageCaptureBuilder Class |
Represents a NXOpen.Gateway.ImageCaptureBuilder builder |
ImageCaptureManager Class |
the ImageCaptureManager class |
PasteBuilder Class |
Represents a NXOpen.Gateway.PasteBuilder |