ImageCaptureBuilderImageSize Enumeration¶
NXOpen.Gateway.ImageCaptureBuilder.ImageSize is an alias for NXOpen.Gateway.ImageCaptureBuilderImageSize
-
class
NXOpen.Gateway.
ImageCaptureBuilderImageSize
¶ Bases:
object
the image size
Enum Members
Enum Member Enum Member Description Pixels16 the 16 pixel size Pixels24 the 24 pixel size Pixels32 the 32 pixel size Pixels48 the 48 pixel size Pixels64 the 64 pixel size Pixels96 the 96 pixel size Pixels128 the 128 pixel size -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-