FloodFillFacetsRule Class¶
-
class
NXOpen.
FloodFillFacetsRule
¶ Bases:
NXOpen.FacetSelectionRule
Represents a
NXOpen.FloodFillFacetsRule
that collects flood filled facets.This rule expands to add all neighboring facets of seed (and the neighbor-neighbors) until the region reaches a closed ring of already collected facets in collector. If already collected facets in collector do not form a closed ring, then the rule expands to all the facets of owning face of the seed. .. versionadded:: NX12.0.0
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the flood fill facets rule: NXOpen.FloodFillFacetsRule |
Method Detail¶
Dispose¶
-
FloodFillFacetsRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX12.0.0.
License requirements: None.
GetData¶
-
FloodFillFacetsRule.
GetData
¶ Gets the data for the flood fill facets rule:
NXOpen.FloodFillFacetsRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (seedFacet, isDeselectionRule) seedFacet is a
NXOpen.IFacet
. seed facet for flood filled facet collection isDeselectionRule is a bool. flag to specify whether it is deselection rule or not. .. versionadded:: NX12.0.0License requirements: gateway (“UG GATEWAY”)