FlatteningBuilderFlatteningConstantType Enumeration¶
NXOpen.FlatteningBuilder.FlatteningConstantType is an alias for NXOpen.FlatteningBuilderFlatteningConstantType
-
class
NXOpen.
FlatteningBuilderFlatteningConstantType
¶ Bases:
object
This enum defines the flattening constraints types.
Enum Members
Enum Member Enum Member Description NoConstraints No constraints ConstantCurveLength Force constant length ConstantFaceArea Force constant area ConstantBodyVolume force constant volume of the body -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-