FlatteningBuilderDistortionMapType Enumeration¶
NXOpen.FlatteningBuilder.DistortionMapType is an alias for NXOpen.FlatteningBuilderDistortionMapType
-
class
NXOpen.
FlatteningBuilderDistortionMapType
¶ Bases:
object
This enum defines the distortion map types.
Enum Members
Enum Member Enum Member Description NotSet no distortion map Length length distortion map Area area distortion map Angle angle distortion map -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-