FineBrushFacetsRule Class¶
-
class
NXOpen.
FineBrushFacetsRule
¶ Bases:
NXOpen.FacetSelectionRule
Represents a
NXOpen.FacetSelectionRule
that collects facets with fine brush tool intent.This rule expands to all neighboring facets of seed (and the neighbor-neighbors) that are inside or crossing brush tool. .. versionadded:: NX12.0.0
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the fine brush facets rule: NXOpen.FineBrushFacetsRule |
Method Detail¶
Dispose¶
-
FineBrushFacetsRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX12.0.0.
License requirements: None.
GetData¶
-
FineBrushFacetsRule.
GetData
¶ Gets the data for the fine brush facets rule:
NXOpen.FineBrushFacetsRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (fineBrushToolStartPoint, fineBrushToolDirection, fineBrushToolRadius, seedFacet) fineBrushToolStartPoint is a
NXOpen.Point3d
. the start point of fine brush tool fineBrushToolDirection is aNXOpen.Vector3d
. the vector defining direction of fine brush tool fineBrushToolRadius is a float. the radius of fine brush tool seedFacet is aNXOpen.IFacet
. the seed facet .. versionadded:: NX12.0.0License requirements: gateway (“UG GATEWAY”)