FileNewTemplateType Enumeration¶
-
class
NXOpen.
FileNewTemplateType
¶ Bases:
object
Enumeration used for templates to determine the type of the template.
Enum Members
Enum Member Enum Member Description Workset Specifies a file new workset template Item Specifies a file new item template DesignElement Specifies a file new design element template DesignControlElement Specifies a file new design control element template DesignFeature Specifies a file new design feature template (actually has no file) Generic Specifies a file new generic non-core template Sheet Specifies a file new sheet template DiagrammingSheetpart Specifies a diagramming sheet part template Last Specifies a last template type. New template types should be inserted before this one -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-