FileNewApplication Enumeration¶
-
class
NXOpen.
FileNewApplication
¶ Bases:
object
The application type of the new file being created through a template
Deprecated since version NX9.0.0: Use
NXOpen.FileNew.GetApplicationNames()
that returns all application names.Enum Members
Enum Member Enum Member Description Drafting Specifies a drafting file new template Modeling Specifies a modeling file new template Studio Specifies a shape studio file new template Assemblies Specifies an assemblies file new template Gateway Specifies a file new template that leaves the new part in Gateway RoutingElectrical Specifies an electrical routing file new template RoutingMechanical Specifies a mechanical routing file new template RoutingLogical Specifies a logical routing file new template Nxsheetmetal Specifies a NX sheet metal file new template SheetTemplate Specifies a drawing sheet template for Insert Sheet dialog CaeFem Specifies a cae fem file new template CaeSim Specifies a cae sim file new template AeroSheetmetal Specifies an Aerospace sheet metal template FlexPcdSheetmetal Specifies a Flex Printed Circuit Design sheet metal template CaeAssyFem Specifies a cae assembly fem file new template Cam Specifies a Manufacturing file new template Inspection Specifies a CMM Inspection file new template Mechatronics Specifies a Mechatronics Concept Designer file new template ShipContainer Specifies an NX Ship Container file new template ShipDetail Specifies an NX Ship Detail file new template ShipReference Specifies an NX Ship Reference file new template ShipSystem Specifies an NX Ship System file new template Welding Specifies an NX Structure Welding Design Control Element template WeldingJoint Specifies an NX Structure Welding Design Feature template Nxle Specifies an NXLE template ShipGaAssembly Specifies an NX Ship GA Assembly file new template ShipGaSystem Specifies an NX Ship GA System file new template Last Specifies the last application type. New application types should be inserted before this one -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-