ComplexScalarFieldWrapper Class |
This class defines a complex value that is internally backed up by a field or two expressions. |
ComplexVectorFieldWrapper Class |
This class defines a complex value that is internally backed up by a field or six expressions. |
DisplayPropertiesBuilder Class |
|
ExportData Class |
Represents data for field export
|
Field Class |
Represents an Field abstract class. |
FieldCollection Class |
Represents a collection of Fields |
FieldDomain Class |
Represents the Field Domains. |
FieldDomainCollection Class |
Provides methods for manipulating the field domains |
FieldDrawHelper Class |
Represents Field_DrawHelper. This class is to be used only for implementing TESTING of Field Display functionality only.
|
FieldEvaluator Class |
|
FieldExpression Class |
Represents the Field Expression class.
|
FieldFormula Class |
Represents the Field Formula class.
|
FieldLink Class |
Represents the Field Link class.
|
FieldLinksTable Class |
Represents the Field LinksTable class.
|
FieldManager Class |
Represents the manager class of the Fields
|
FieldReference Class |
Represents an reference field
|
FieldTable Class |
Represents the Field Table class.
|
FieldVariable Class |
Represents the Field Variables
|
FieldWrapper Class |
This class defines a value that is internally backed up by a field. |
IApplication Class |
Interface for all applications registered with the Field subsystem. Each application type should only be registered once with the Field subsystem. Each application class is identified by its name. |
IApplicationData Class |
Interface for all application specific data to be registered on fields. Only one application specific data object per IApplication can be added on a field. |
ImportData Class |
Represents data transfer objectst for field import
|
NameVariable Class |
This class stores the common name and measure for field variables. |
PathObjects Class |
Contains objects that define a lattice path
|
PathObjectsList Class |
Represents a list of objects. |
ScalarFieldWrapper Class |
This class defines a scalar value that is internally backed up by a (optionally scaled) field or an expression. |
SpatialMap Class |
Represents the Field Domain Map
|
SpatialMapBuilder Class |
|
VectorFieldWrapper Class |
This class defines a vector value that is internally backed up by a (optionally scaled) field or three expressions. |