FieldVariableType Enumeration

NXOpen.Fields.FieldVariable.Type is an alias for NXOpen.Fields.FieldVariableType

class NXOpen.Fields.FieldVariableType

Bases: object

Variable Types

Enum Members

Enum Member Enum Member Description
Unknown
Independent
Dependent
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.