FieldVariableBounds_Struct Struct

NXOpen.Fields.FieldVariable.Bounds is an alias for NXOpen.Fields.FieldVariableBounds_Struct

class NXOpen.Fields.FieldVariableBounds_Struct

Bases: object

Variable Bounds structure .

Constructor: NXOpen.Fields.FieldVariable.Bounds()

Fields

Field Description
IsMinimumDefined true if minimum bound is defined
IsMinimumInclusive true if minimum bound is inclusive
MinimumValue minimum bound value
IsMaximumDefined true if maximum bound is defined
IsMaximumInclusive true if maximum bound is inclusive
MaximumValue maximum bound value

IsMinimumDefined

FieldVariableBounds_Struct.IsMinimumDefined

true if minimum bound is defined -------------------------------------

Field Value Type:bool

IsMinimumInclusive

FieldVariableBounds_Struct.IsMinimumInclusive

true if minimum bound is inclusive -------------------------------------

Field Value Type:bool

MinimumValue

FieldVariableBounds_Struct.MinimumValue

minimum bound value -------------------------------------

Field Value Type:float

IsMaximumDefined

FieldVariableBounds_Struct.IsMaximumDefined

true if maximum bound is defined -------------------------------------

Field Value Type:bool

IsMaximumInclusive

FieldVariableBounds_Struct.IsMaximumInclusive

true if maximum bound is inclusive -------------------------------------

Field Value Type:bool

MaximumValue

FieldVariableBounds_Struct.MaximumValue

maximum bound value -------------------------------------

Field Value Type:float