FieldEvaluatorLinearLogOptionEnum Enumeration¶
NXOpen.Fields.FieldEvaluator.LinearLogOptionEnum is an alias for NXOpen.Fields.FieldEvaluatorLinearLogOptionEnum
-
class
NXOpen.Fields.
FieldEvaluatorLinearLogOptionEnum
¶ Bases:
object
Log Options for Linear interpolator
Enum Members
Enum Member Enum Member Description LinearLinear Standard linear interpolation. Both Independent variable and Dependent variable scaling are linear LogLinear Independent variable scaling is logarithmic (ln), Dependent variable scaling is linear LinearLog Independent variable scaling is linear, Dependent variable scaling is logarithmic (ln) LogLog Both Independent variable and Dependent variable scaling are logarithmic (ln) -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-