FieldEvaluatorInverseDistanceWeightingEnum Enumeration¶
NXOpen.Fields.FieldEvaluator.InverseDistanceWeightingEnum is an alias for NXOpen.Fields.FieldEvaluatorInverseDistanceWeightingEnum
-
class
NXOpen.Fields.
FieldEvaluatorInverseDistanceWeightingEnum
¶ Bases:
object
Options for IDW (inverse weighted distance) interpolator
Enum Members
Enum Member Enum Member Description All Sum of the weighted value of all points, based on the inverse of the distance Radius Sum of the weighted value of points within a radius (as a fraction of the bounding box diagonal), based on the inverse of the distance NearestPoints Sum of the weighted value of N nearest points (as a fraction of the total number of points), based on the inverse of the distance -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-