FieldEvaluatorInterpolationEnum Enumeration¶
NXOpen.Fields.FieldEvaluator.InterpolationEnum is an alias for NXOpen.Fields.FieldEvaluatorInterpolationEnum
-
class
NXOpen.Fields.
FieldEvaluatorInterpolationEnum
¶ Bases:
object
Interpolation type
Enum Members
Enum Member Enum Member Description NotSet No interpolation method; table can only be used as a lookup Linear1d Standard linear interpolation between bounding points NearestNeighbor1d Locates the nearest point and returns its value InverseDistanceWeighting1d Sum of the weighted value of all points, based on the inverse of the distance Delaunay2dFast Triangulates the independent values and uses the bounding triangle, sacrifices accuracy for speed Delaunay2dMedium Triangulates the independent values and uses the bounding triangle, compromise between accuracy and speed Delaunay2dAccurate Triangulates the independent values and uses the bounding triangle, sacrifices speed for accuracy NearestNeighbor2d Locates the nearest point in a plane and returns its value RenkaShepard2d Refined inverse distance weighting in 2D space InverseDistanceWeighting2d Sum of the weighted value of all points in 2D space, based on the inverse of the distance Delaunay3dFast Creates Tetrahedrals using the independent values and uses the bounding tetrahedron, sacrifices accuracy for speed Delaunay3dMedium Creates Tetrahedrals using the independent values and uses the bounding tetrahedron, compromise between accuracy and speed Delaunay3dAccurate Creates Tetrahedrals using the independent values and uses the bounding tetrahedron, sacrifices speed for accuracy NearestNeighbor3d Locates the nearest point in space and returns its value RenkaShepard3d Refined inverse distance weighting in 3D space InverseDistanceWeighting3d Sum of the weighted value of all points in 3D space, based on the inverse of the distance NearestNeighborNd Locates the nearest point in N dimensional space and returns its value RenkaShepardNd Refined inverse distance weighting in N dimensional space InverseDistanceWeightingNd Sum of the weighted value of all points in N dimensional, based on the inverse of the distance ApproxNearestNeighbor2d Locates the approximate nearest point in a plane and returns its value ApproxNearestNeighbor3d Locates the approximate nearest point in space and returns its value ApproxNearestNeighborNd Locates the approximate nearest point in N dimensional space and returns its value Akima1d akima interpolation Akima721d akima72 interpolation Cubic1d cubic interpolation Bilinear2d linear interpolation in both directions Biakima2d akima interpolation in both directions Biakima722d akima72 interpolation in both directions Bicubic2d cubic interpolation in both directions AkimaLinear2d akima interpolation in x direction, linear in y direction Akima72Linear2d akima72 interpolation in x direction, linear in y direction CubicLinear2d cubic interpolation in x direction, linear in y direction -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-