ExportData Class¶
-
class
NXOpen.Fields.
ExportData
¶ Bases:
NXOpen.TransientObject
Represents data for field export
To create a new instance of this class, use
NXOpen.Fields.FieldManager.CreateExportData()
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
AddField | Add a field |
AddFields | Add a field |
Dispose | Destroys the object |
GetFields | Gets the fields |
GetFileName | Get file name |
SetFileName | Set file name |
Method Detail¶
AddField¶
-
ExportData.
AddField
¶ Add a field
Signature
AddField(field)
Parameters: field ( NXOpen.Fields.Field
) – field to addNew in version NX6.0.0.
License requirements: None.
AddFields¶
-
ExportData.
AddFields
¶ Add a field
Signature
AddFields(fields)
Parameters: fields (list of NXOpen.Fields.Field
) – fields to addNew in version NX6.0.0.
License requirements: None.
Dispose¶
-
ExportData.
Dispose
¶ Destroys the object
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.
GetFields¶
-
ExportData.
GetFields
¶ Gets the fields
Signature
GetFields()
Returns: fields Return type: list of NXOpen.Fields.Field
New in version NX6.0.0.
License requirements: None.