DisplayPropertiesBuilderTblPointTypeEnum Enumeration

NXOpen.Fields.DisplayPropertiesBuilder.TblPointTypeEnum is an alias for NXOpen.Fields.DisplayPropertiesBuilderTblPointTypeEnum

class NXOpen.Fields.DisplayPropertiesBuilderTblPointTypeEnum

Bases: object

Field Tbl Point Type

Enum Members

Enum Member Enum Member Description
Hide
Show
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.