DisplayPropertiesBuilderFieldQuantityType Enumeration¶
NXOpen.Fields.DisplayPropertiesBuilder.FieldQuantityType is an alias for NXOpen.Fields.DisplayPropertiesBuilderFieldQuantityType
-
class
NXOpen.Fields.
DisplayPropertiesBuilderFieldQuantityType
¶ Bases:
object
Field Quanity Type
Enum Members
Enum Member Enum Member Description Type0 Type1 Type2 Type3 Type4 Type5 Type6 Type7 Type8 Type9 Type10 Type11 Type12 Type13 Type14 Type15 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-