DisplayPropertiesBuilderDepLabelValueEnum Enumeration

NXOpen.Fields.DisplayPropertiesBuilder.DepLabelValueEnum is an alias for NXOpen.Fields.DisplayPropertiesBuilderDepLabelValueEnum

class NXOpen.Fields.DisplayPropertiesBuilderDepLabelValueEnum

Bases: object

Field Dep Label Value

Enum Members

Enum Member Enum Member Description
NotSet
MinimumMaximum
Maximum
Minimum
All
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.