WaveInterfaceLinkerBuilder Class¶
-
class
NXOpen.Features.
WaveInterfaceLinkerBuilder
¶ Bases:
NXOpen.Builder
Represents a WaveInterfacelinker Feature builder
To create a new instance of this class, use
NXOpen.Features.BaseFeatureCollection.CreateWaveInterfaceLinkerBuilder()
Default values.
Property Value Associative 1 CopyThreads 1 InheritDisplayProperties 0 MakePositionIndependent 0 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative |
CopyThreads | Returns or sets the copy threads |
DisplayReferenceGeometry | Returns or sets the setting that controls whether or not the reference geometry in the linked product interface are displayed |
InheritDisplayProperties | Returns or sets the inherit display properties |
MakePositionIndependent | Returns or sets the make position independent |
SourcePartOccurrence | Returns or sets the source part occurrence |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ClearAll | Clear all selected objects |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
InsertObjects | Insert selected objects |
RemoveObjects | Remove unselected objects |
SetALL | Set all objects as chosen |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Associative¶
-
WaveInterfaceLinkerBuilder.
Associative
¶ Returns or sets the associative
-------------------------------------
Getter Method
Signature
Associative
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative
Parameters: associative (bool) – New in version NX9.0.0.
License requirements: None.
CopyThreads¶
-
WaveInterfaceLinkerBuilder.
CopyThreads
¶ Returns or sets the copy threads
-------------------------------------
Getter Method
Signature
CopyThreads
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopyThreads
Parameters: copyThreads (bool) – New in version NX9.0.0.
License requirements: None.
DisplayReferenceGeometry¶
-
WaveInterfaceLinkerBuilder.
DisplayReferenceGeometry
¶ Returns or sets the setting that controls whether or not the reference geometry in the linked product interface are displayed
-------------------------------------
Getter Method
Signature
DisplayReferenceGeometry
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayReferenceGeometry
Parameters: displayReferenceGeometry (bool) – New in version NX11.0.1.
License requirements: None.
InheritDisplayProperties¶
-
WaveInterfaceLinkerBuilder.
InheritDisplayProperties
¶ Returns or sets the inherit display properties
-------------------------------------
Getter Method
Signature
InheritDisplayProperties
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InheritDisplayProperties
Parameters: inheritDisplayProperties (bool) – New in version NX9.0.0.
License requirements: None.
MakePositionIndependent¶
-
WaveInterfaceLinkerBuilder.
MakePositionIndependent
¶ Returns or sets the make position independent
-------------------------------------
Getter Method
Signature
MakePositionIndependent
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MakePositionIndependent
Parameters: makePositionIndependent (bool) – New in version NX9.0.0.
License requirements: None.
SourcePartOccurrence¶
-
WaveInterfaceLinkerBuilder.
SourcePartOccurrence
¶ Returns or sets the source part occurrence
-------------------------------------
Getter Method
Signature
SourcePartOccurrence
Returns: Return type: NXOpen.TaggedObject
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SourcePartOccurrence
Parameters: sourcePartOcc ( NXOpen.TaggedObject
) –New in version NX9.0.0.
License requirements: None.
Method Detail¶
ClearAll¶
-
WaveInterfaceLinkerBuilder.
ClearAll
¶ Clear all selected objects
Signature
ClearAll()
New in version NX9.0.0.
License requirements: None.
InsertObjects¶
-
WaveInterfaceLinkerBuilder.
InsertObjects
¶ Insert selected objects
Signature
InsertObjects(selectedObjects)
Parameters: selectedObjects (list of NXOpen.TaggedObject
) – items in listNew in version NX9.0.0.
License requirements: None.
RemoveObjects¶
-
WaveInterfaceLinkerBuilder.
RemoveObjects
¶ Remove unselected objects
Signature
RemoveObjects(removedObjects)
Parameters: removedObjects (list of NXOpen.TaggedObject
) – items in listNew in version NX9.0.0.
License requirements: None.
SetALL¶
-
WaveInterfaceLinkerBuilder.
SetALL
¶ Set all objects as chosen
Signature
SetALL()
New in version NX9.0.0.
License requirements: None.
Validate¶
-
WaveInterfaceLinkerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.