AllAroundVisionBuilderTypes Enumeration |
Used to indicate the type of obstructing geometry to use. |
AllAroundVisionBuilderWindowTypes Enumeration |
Used to indicate the type of geometry used to define the window. |
BaseDataImportExportBuilderExportOptions Enumeration |
This enum represents the option to indicate if the expressions are to be exported to a new item or an existing item in Teamcenter. |
BaseDataImportExportBuilderOperateOptions Enumeration |
This enum represents the import or export operate options |
BaseDataLoadingBuilderLoadingType Enumeration |
This enum represents the vehicle loading types. |
BaseDataLoadingWheelBuilderDataDefinitionOptions Enumeration |
This enum represents the options to define the wheel position. |
BaseDataPassengerBuilderSeatDirectionOptions Enumeration |
This enum represents the options to define the passenger’s seat direction type. |
BaseDataSourceBuilderBaseDataSourceOption Enumeration |
Represents the base data source option, you can select one component or display part which contains the Base Data feature group for current work part. |
BaseDataWheelBuilderPositionDefinitionOptions Enumeration |
This enum represents the options to define the wheel position. |
BumperPendulumBuilderRequirementsControlType Enumeration |
Represents the requirements control types to define the bumper pendulum. |
BumperPendulumBuilderVisualizationType Enumeration |
Represents the visualization types of the output. |
CloseRangeCameraListItemBuilderTypes Enumeration |
This enum represents the camera definition options to define the close range visibility. |
CloseRangeDemoCylinderListItemBuilderValidateTypes Enumeration |
This enum represents the simple or detailed checking options to validate demo cylinders visibility. |
CloseRangeVisibilityBuilderEyePointOffsetTypes Enumeration |
This enum represents the eye position offset options. |
CloseRangeVisibilityBuilderEyePointTypes Enumeration |
This enum represents the binocular or monocular eye position definition options. |
CloseRangeVisibilityBuilderPathPositionTypes Enumeration |
This enum represents the cylinder path position display options. |
CloseRangeVisibilityBuilderPositionMethods Enumeration |
This enum represents the cylinder position method options. |
CloseRangeVisibilityBuilderPositionPaths Enumeration |
This enum represents the cylinder position path options. |
CloseRangeVisibilityBuilderRequirementsControlType Enumeration |
This enum represents the standard or user defined requirement options. |
CrashBarrierBuilderCrossPositionType Enumeration |
Represents the cross position types. |
CrashBarrierBuilderOverlapSideType Enumeration |
Represents the overlap side types for the front and rear barriers. |
CrashBarrierBuilderPositionObjectType Enumeration |
Represents the position object types. |
CrashBarrierBuilderRequirementsControlsControlType Enumeration |
Represents the requirements control types to define the crash barrier. |
CrashBarrierBuilderShapeType Enumeration |
Represents the shape types. |
CrashBarrierBuilderSideOverlapSideType Enumeration |
Represents the overlap side types for side barrier. |
CrashBarrierBuilderSidePositionType Enumeration |
Represents the position types for side barrier. |
DynamicCurbBuilderMethodType Enumeration |
Represents the type of inner line to create dynamic curb. |
DynamicCurbBuilderPositionType Enumeration |
Represents the dynamic curb positions. |
DynamicCurbBuilderRequirementsControlType Enumeration |
Represents the requirements control types to define the dynamic curb. |
DynamicCurbBuilderVisualizationType Enumeration |
Represents the visualization types of the output. |
DynamicCurbBuilderWheelType Enumeration |
Represents the type of the wheel size option for dynamic curb. |
GroundClearanceBuilderPositionType Enumeration |
Represents the ground clearance positions. |
GroundClearanceBuilderRequirementControls Enumeration |
This enum represents the standard or user defined requirement options for ground clearance. |
GroundClearanceBuilderSectionCurveType Enumeration |
Represents the type of under axle section curve type to create ground clearace. |
GroundClearanceBuilderSurfaceLengthType Enumeration |
Represents the type of general surface length to create ground clearace. |
GroundClearanceBuilderVisualizationTypes Enumeration |
This enum represents the output definition options. |
GroundClearanceBuilderWheelType Enumeration |
Represents the type of the wheel size option for ground clearance. |
HeadImpactAPillarDetailBuilderMeasurementMethodType Enumeration |
Represents the measurement methods used to position point 1. |
HeadImpactBuilderCalculationType Enumeration |
Represents the calculation types. |
HeadImpactBuilderRequirementsControlType Enumeration |
Represents the requirements control types. |
InnerAngleBuilderCalculationMethodType Enumeration |
Represents the calculation method types to calculate inner angle output. |
InnerAngleBuilderRequirementsControlType Enumeration |
Represents the requirements control types to define the inner angle. |
InnerAngleBuilderVisualizationType Enumeration |
Represents the visualization types of the output. |
InnerAngleBuilderWheelSizeType Enumeration |
Represents the wheel size types to calculate inner angle output. |
ManikinBuilderClassificationType Enumeration |
the vehicle classification type |
ManikinBuilderPositionType Enumeration |
the vehicle seat position type |
ManikinBuilderSAEPercentileType Enumeration |
the vehicle percentile type |
ManikinBuilderStandardType Enumeration |
the vehicle standard type |
MirrorCertificationBuilderDriverSideStandardsType Enumeration |
Used to indicate the standard for the driver mirror. |
MirrorCertificationBuilderEyeFromOptionType Enumeration |
Used to indicate what part the eye is from. |
MirrorCertificationBuilderEyeMethodType Enumeration |
Used to indicate the method to calculate the eye location based on the distance from the eyellipse to the mirror pivot. |
MirrorCertificationBuilderEyePointMethodType Enumeration |
Used to indicate the method to define the eye point. |
MirrorCertificationBuilderEyellipsePercentileType Enumeration |
Used to indicate the eyellipse percentile that is used in mirror certification. |
MirrorCertificationBuilderInsideStandardsType Enumeration |
Used to indicate the standard for the inside mirror. |
MirrorCertificationBuilderInstructionFieldPositionType Enumeration |
Used to indicate the postion where the instruction field will be. |
MirrorCertificationBuilderInstructionFieldsType Enumeration |
Used to indicate the shape type of the instruction field. |
MirrorCertificationBuilderLocationType Enumeration |
Used to indicate the mirror location. |
MirrorCertificationBuilderMirrorOrientationType Enumeration |
Used to indicate the method to rotate mirror. |
MirrorCertificationBuilderMirrorSurfaceType Enumeration |
Used to indicate the mirror surface type. |
MirrorCertificationBuilderPassengerSideStandardsType Enumeration |
Used to indicate the standard for the passenger mirror. |
MirrorCertificationBuilderShowVisionConeType Enumeration |
Used to indicate what vision cone will be shown. |
OilPanBuilderPositionType Enumeration |
Represents the oil pan positions. |
OilPanBuilderRequirementsControlType Enumeration |
Represents the requirements control types to define the oil pan. |
OilPanBuilderVisualizationType Enumeration |
Represents the visualization types of the output. |
PedestrianProtectionBuilderFont Enumeration |
Settings for font to create the various output with |
PedestrianProtectionBuilderInternalBumperType Enumeration |
Settings for the type of pedestrian protection internal bumper line method to use in the study |
PedestrianProtectionBuilderStandardType Enumeration |
Settings for the type of pedestrian protection standard to use in the study |
PedestrianProtectionBuilderTransformMethods Enumeration |
Settings for the transform method of pedestrian protection active hood system |
PedestrianProtectionBuilderTypes Enumeration |
Settings for the type of pedestrian protection impact study |
PedestrianProtectionBuilderWad Enumeration |
Settings for the start, end and boundary wrap around distance line to create |
PedestrianProtectionBuilderWidth Enumeration |
Settings for width to create the various output with |
PendulumPlacementBuilderLocationType Enumeration |
This enum represents the pendulum placement location options. |
PendulumPlacementBuilderPendulumProfileType Enumeration |
This enum represents the pendulum placement profile options. |
PendulumPlacementBuilderPositionMethodType Enumeration |
This enum represents the pendulum placement method options. |
PendulumPlacementBuilderSideType Enumeration |
This enum represents the pendulum placement side options. |
ReflectionDataBuilderReflectMethodType Enumeration |
the reflection data option type |
ReflectionDataBuilderResolutionType Enumeration |
the resolution type |
SeatBeltAnchorageBuilderATLType Enumeration |
the show ATL type |
SeatBeltAnchorageBuilderAnchorageLocationTypes Enumeration |
the seat belt anchorage location type |
SeatBeltAnchorageBuilderLOneLimitType Enumeration |
the lone limit type |
SeatBeltAnchorageBuilderLTwoLimitType Enumeration |
the ltwo limit type |
SeatBeltAnchorageBuilderLowerAreaType Enumeration |
the lower area type |
SeatBeltAnchorageBuilderLowerLimitType Enumeration |
the lower limit type |
SeatBeltAnchorageBuilderRoutingTypes Enumeration |
the seat belt routing type |
SeatBeltAnchorageBuilderSeatPositionTypes Enumeration |
the seat position type |
SeatBeltAnchorageBuilderSeatTypes Enumeration |
the seat type |
SeatBeltAnchorageBuilderStandardTypes Enumeration |
the standard type |
SeatBeltAnchorageBuilderUpperAreaType Enumeration |
the upper area type |
SlopeBuilderPositionType Enumeration |
Represents the slope positions. |
SlopeBuilderRequirementsControlType Enumeration |
Represents the requirements control types to define the slope. |
SlopeBuilderVisualizationType Enumeration |
Represents the visualization types of the output. |
SlopeBuilderWheelSizeType Enumeration |
Represents the wheel size types to calculate slope output. |
StaticCurbBuilderPositionType Enumeration |
Represents the static curb positions. |
StaticCurbBuilderRequirementsControlType Enumeration |
Represents the requirements control types to define the static curb. |
StaticCurbBuilderVisualizationType Enumeration |
Represents the visualization types of the output. |
TireEnvelopeBuilderDriverGraphOption Enumeration |
Settings to indicate the driver definition to use with the MacPherson Strut suspension template. |
TireEnvelopeBuilderEnvelopeOffsetMethod Enumeration |
Settings to indicate how the offset will be defined. |
TireEnvelopeBuilderMotionMethod Enumeration |
Settings to indicate how the suspension system motion will be defined. |
TireEnvelopeBuilderSpindleFileLocationOption Enumeration |
Settings to indicate the location to select the spindle file. |
TireEnvelopeBuilderSuspensionTemplateType Enumeration |
Settings to indicate the defined suspension template to use. |
TireEnvelopeBuilderTireDefinitionOption Enumeration |
Settings to indicate how the tire profile will be defined. |
VehicleCoordinateSystemBuilderTypes Enumeration |
Vehicle Coordinate System type |
VisionPlaneBuilderCustomVisionAngle Enumeration |
Represents the vision angle type to define the Vision Plane. |
VisionPlaneBuilderEnumEyeType Enumeration |
Represents the eye definition type to define the Vision Plane. |
WheelCoveringBuilderPositionType Enumeration |
Represents the wheel covering positions. |
WheelCoveringBuilderRequirementsControlType Enumeration |
Represents the requirements control types to define the wheel covering. |
WheelCoveringBuilderSurfacePlaneType Enumeration |
Represents the type of the surface plane. |
WheelCoveringBuilderSurfaceSectionType Enumeration |
Represents the type of the surface section. |
WheelFixingBuilderObjectPositionType Enumeration |
Represents the object position used to indicate if the wheel fixing is positioned at the theoretically widest dimension of the wheel (diameter) or exactly at the wheel geometry of the base data. |
WheelFixingBuilderPositionType Enumeration |
Represents the wheel fixing positions. |
WheelFixingBuilderRequirementsControlType Enumeration |
Represents the requirements control types to define the wheel fixing. |
WheelFixingBuilderShapeType Enumeration |
Represents the shape used to indicate if the wheel fixing is a block or a circle segment. |
WheelFixingBuilderWheelSizeType Enumeration |
Represents the wheel size used to indicate if the wheel fixing is based on static radius or the diameter of the wheels. |
WindshieldDatumBuilderCustomVisionAngle Enumeration |
Represents the vision angle type to define the Windshield Datum. |
WindshieldDatumBuilderEnumEyeType Enumeration |
Represents the eye definition type to define the Windshield Datum. |