TireEnvelopeBuilderTireDefinitionOption Enumeration¶
NXOpen.Features.VehicleDesign.TireEnvelopeBuilder.TireDefinitionOption is an alias for NXOpen.Features.VehicleDesign.TireEnvelopeBuilderTireDefinitionOption
-
class
NXOpen.Features.VehicleDesign.
TireEnvelopeBuilderTireDefinitionOption
¶ Bases:
object
Settings to indicate how the tire profile will be defined.
Enum Members
Enum Member Enum Member Description SolidBody Use a solid body. ProfileCurves Use curves in the current work part. SketchfromOtherPart Use curves from a sketch in another part. ProfilePointFile Read a text file with tire profile points. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-