TireEnvelopeBuilderDriverGraphOption Enumeration¶
NXOpen.Features.VehicleDesign.TireEnvelopeBuilder.DriverGraphOption is an alias for NXOpen.Features.VehicleDesign.TireEnvelopeBuilderDriverGraphOption
-
class
NXOpen.Features.VehicleDesign.
TireEnvelopeBuilderDriverGraphOption
¶ Bases:
object
Settings to indicate the driver definition to use with the MacPherson Strut suspension template.
Enum Members
Enum Member Enum Member Description RectangularJounceRebound Use the rectangular jounce rebound definition. RectangularTaperedY Use the rectangular definition with taper in the Y direction. RectangularTaperedX Use the rectangular definition with taper in the X direction. TaperedOneSide Use the rectangular definition with taper on one side. BySketch Use a sketch to define the driver. TwoDriversOneFixed Use a fixed definition for two drivers. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-