StaticCurbBuilderPositionType Enumeration

NXOpen.Features.VehicleDesign.StaticCurbBuilder.PositionType is an alias for NXOpen.Features.VehicleDesign.StaticCurbBuilderPositionType

class NXOpen.Features.VehicleDesign.StaticCurbBuilderPositionType

Bases: object

Represents the static curb positions.

Enum Members

Enum Member Enum Member Description
Front Front
Rear Rear
Both Both
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.