SeatBeltAnchorageBuilderLowerLimitType Enumeration¶
NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilder.LowerLimitType is an alias for NXOpen.Features.VehicleDesign.SeatBeltAnchorageBuilderLowerLimitType
-
class
NXOpen.Features.VehicleDesign.
SeatBeltAnchorageBuilderLowerLimitType
¶ Bases:
object
the lower limit type
Enum Members
Enum Member Enum Member Description Length450 lower limit distance of 450 Length500 lower limit distance of 500 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-