PendulumPlacementBuilderPendulumProfileType Enumeration

NXOpen.Features.VehicleDesign.PendulumPlacementBuilder.PendulumProfileType is an alias for NXOpen.Features.VehicleDesign.PendulumPlacementBuilderPendulumProfileType

class NXOpen.Features.VehicleDesign.PendulumPlacementBuilderPendulumProfileType

Bases: object

This enum represents the pendulum placement profile options.

Enum Members

Enum Member Enum Member Description
Eu
Us
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.