PedestrianProtectionBuilderWidth Enumeration¶
NXOpen.Features.VehicleDesign.PedestrianProtectionBuilder.Width is an alias for NXOpen.Features.VehicleDesign.PedestrianProtectionBuilderWidth
-
class
NXOpen.Features.VehicleDesign.
PedestrianProtectionBuilderWidth
¶ Bases:
object
Settings for width to create the various output with
Enum Members
Enum Member Enum Member Description Default Default Width Normal normal Width Thick Thick width Thin Thin width One Two Three Four Five Six Seven Eight Nine -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-