PedestrianProtectionBuilderFont Enumeration¶
NXOpen.Features.VehicleDesign.PedestrianProtectionBuilder.Font is an alias for NXOpen.Features.VehicleDesign.PedestrianProtectionBuilderFont
-
class
NXOpen.Features.VehicleDesign.
PedestrianProtectionBuilderFont
¶ Bases:
object
Settings for font to create the various output with
Enum Members
Enum Member Enum Member Description Default Default Font Solid Solid Font Dashed Dashed Font Phantom Phantom Font Centerline Centerline Font Dotted Dotted Font LongDashed LongDashed Font DottedDashed DottedDashed Font -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-