ManikinBuilderStandardType Enumeration

NXOpen.Features.VehicleDesign.ManikinBuilder.StandardType is an alias for NXOpen.Features.VehicleDesign.ManikinBuilderStandardType

class NXOpen.Features.VehicleDesign.ManikinBuilderStandardType

Bases: object

the vehicle standard type

Enum Members

Enum Member Enum Member Description
SAEJ826Jul1995 1995 SAE j826 Standard Type
Saej833 SAE j833 Standard Type
UserDefined User Defined Manikin Size Type
SAEJ826Nov2008 2008 SAE j826 Standard Type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.