ManikinBuilderPositionType Enumeration

NXOpen.Features.VehicleDesign.ManikinBuilder.PositionType is an alias for NXOpen.Features.VehicleDesign.ManikinBuilderPositionType

class NXOpen.Features.VehicleDesign.ManikinBuilderPositionType

Bases: object

the vehicle seat position type

Enum Members

Enum Member Enum Member Description
Driver Driver Type
Passenger Passenger Type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.