ManikinBuilderClassificationType Enumeration¶
NXOpen.Features.VehicleDesign.ManikinBuilder.ClassificationType is an alias for NXOpen.Features.VehicleDesign.ManikinBuilderClassificationType
-
class
NXOpen.Features.VehicleDesign.
ManikinBuilderClassificationType
¶ Bases:
object
the vehicle classification type
Enum Members
Enum Member Enum Member Description ClassA Class A Classification Type. The type of vehicles includes passenger cars, vans, and light trucks. ClassB Class B Classification Type. The type of vehicles includes heavy trucks, some buses and multipurpose passenger vehicles. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-