HeadImpactUpperRoofDetailBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
HeadImpactUpperRoofDetailBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Features.VehicleDesign.HeadImpactUpperRoofDetailBuilder
.This is an abstract class and cannot be instantiated.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CreateGeometry | Returns or sets the create construction geometry flag. |
D1 | Returns the calculated horizontal distance between plane A and plane B. |
D2 | Returns the calculated horizontal distance between plane C and plane D. |
PointA | Returns or sets the point A additional geometry. |
PointAFlag | Returns or sets the point A additional geometry flag. |
PointB | Returns or sets the point B additional geometry. |
PointBFlag | Returns or sets the point B additional geometry flag. |
PointC | Returns or sets the point C additional geometry. |
PointCFlag | Returns or sets the point C additional geometry flag. |
PointD | Returns or sets the point D additional geometry. |
PointDFlag | Returns or sets the point D additional geometry flag. |
PointM | Returns or sets the point M alternative point. |
PointMFlag | Returns or sets the point M alternative point flag. |
ReqVerticalMax | Returns the vertical maximum required approach angle. |
ReqVerticalMin | Returns the vertical minimum required approach angle. |
RoofOffset | Returns the offset used to position point C and point D. |
RoofRatio | Returns the ratio used to locate planes E, F, G, and H. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CreateGeometry¶
-
HeadImpactUpperRoofDetailBuilder.
CreateGeometry
¶ Returns or sets the create construction geometry flag.
-------------------------------------
Getter Method
Signature
CreateGeometry
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateGeometry
Parameters: createGeometry (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
D1¶
-
HeadImpactUpperRoofDetailBuilder.
D1
¶ Returns the calculated horizontal distance between plane A and plane B.
-------------------------------------
Getter Method
Signature
D1
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
D2¶
-
HeadImpactUpperRoofDetailBuilder.
D2
¶ Returns the calculated horizontal distance between plane C and plane D.
-------------------------------------
Getter Method
Signature
D2
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
PointA¶
-
HeadImpactUpperRoofDetailBuilder.
PointA
¶ Returns or sets the point A additional geometry.
-------------------------------------
Getter Method
Signature
PointA
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointA
Parameters: pointA ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointAFlag¶
-
HeadImpactUpperRoofDetailBuilder.
PointAFlag
¶ Returns or sets the point A additional geometry flag.
-------------------------------------
Getter Method
Signature
PointAFlag
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointAFlag
Parameters: pointAFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointB¶
-
HeadImpactUpperRoofDetailBuilder.
PointB
¶ Returns or sets the point B additional geometry.
-------------------------------------
Getter Method
Signature
PointB
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointB
Parameters: pointB ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointBFlag¶
-
HeadImpactUpperRoofDetailBuilder.
PointBFlag
¶ Returns or sets the point B additional geometry flag.
-------------------------------------
Getter Method
Signature
PointBFlag
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointBFlag
Parameters: pointBFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointC¶
-
HeadImpactUpperRoofDetailBuilder.
PointC
¶ Returns or sets the point C additional geometry.
-------------------------------------
Getter Method
Signature
PointC
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointC
Parameters: pointC ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointCFlag¶
-
HeadImpactUpperRoofDetailBuilder.
PointCFlag
¶ Returns or sets the point C additional geometry flag.
-------------------------------------
Getter Method
Signature
PointCFlag
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointCFlag
Parameters: pointCFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointD¶
-
HeadImpactUpperRoofDetailBuilder.
PointD
¶ Returns or sets the point D additional geometry.
-------------------------------------
Getter Method
Signature
PointD
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointD
Parameters: pointD ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointDFlag¶
-
HeadImpactUpperRoofDetailBuilder.
PointDFlag
¶ Returns or sets the point D additional geometry flag.
-------------------------------------
Getter Method
Signature
PointDFlag
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointDFlag
Parameters: pointDFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointM¶
-
HeadImpactUpperRoofDetailBuilder.
PointM
¶ Returns or sets the point M alternative point.
-------------------------------------
Getter Method
Signature
PointM
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointM
Parameters: pointM ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PointMFlag¶
-
HeadImpactUpperRoofDetailBuilder.
PointMFlag
¶ Returns or sets the point M alternative point flag.
-------------------------------------
Getter Method
Signature
PointMFlag
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointMFlag
Parameters: pointMFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ReqVerticalMax¶
-
HeadImpactUpperRoofDetailBuilder.
ReqVerticalMax
¶ Returns the vertical maximum required approach angle.
-------------------------------------
Getter Method
Signature
ReqVerticalMax
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ReqVerticalMin¶
-
HeadImpactUpperRoofDetailBuilder.
ReqVerticalMin
¶ Returns the vertical minimum required approach angle.
-------------------------------------
Getter Method
Signature
ReqVerticalMin
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
RoofOffset¶
-
HeadImpactUpperRoofDetailBuilder.
RoofOffset
¶ Returns the offset used to position point C and point D.
-------------------------------------
Getter Method
Signature
RoofOffset
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
RoofRatio¶
-
HeadImpactUpperRoofDetailBuilder.
RoofRatio
¶ Returns the ratio used to locate planes E, F, G, and H.
-------------------------------------
Getter Method
Signature
RoofRatio
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
HeadImpactUpperRoofDetailBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.