HeadImpactSideRailDetailBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
HeadImpactSideRailDetailBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder
.This is an abstract class and cannot be instantiated.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CreateGeometry | Returns or sets the create construction geometry flag. |
PT11Left | Returns or sets the left PT11 additional geometry. |
PT11LeftFlag | Returns or sets the left PT11 additional geometry flag. |
PT11Right | Returns or sets the right PT11 additional geometry. |
PT11RightFlag | Returns or sets the right PT11 additional geometry flag. |
PT12Left | Returns or sets the left PT12 additional geometry. |
PT12LeftFlag | Returns or sets the left PT12 additional geometry flag. |
PT12Right | Returns or sets the right PT12 additional geometry. |
PT12RightFlag | Returns or sets the right PT12 additional geometry flag. |
PT14Left | Returns or sets the left PT14 additional geometry. |
PT14LeftFlag | Returns or sets the left PT14 additional geometry flag. |
PT14Right | Returns or sets the right PT14 additional geometry. |
PT14RightFlag | Returns or sets the right PT14 additional geometry flag. |
ReqHorizontalLeftExact | Returns the left horizontal required approach angle. |
ReqHorizontalRightExact | Returns the right horizontal required approach angle. |
ReqVerticalMax | Returns the vertical maximum required approach angle. |
ReqVerticalMin | Returns the vertical minimum required approach angle. |
SR1Left | Returns or sets the left SR1 alternative point. |
SR1LeftFlag | Returns or sets the left SR1 alternative point flag. |
SR1Offset | Returns the offset used to position SR1. |
SR1Right | Returns or sets the right SR1 alternative point. |
SR1RightFlag | Returns or sets the right SR1 alternative point flag. |
SR2ALeft | Returns or sets the left SR2A alternative point. |
SR2ALeftFlag | Returns or sets the left SR2A alternative point flag. |
SR2ARight | Returns or sets the right SR2A alternative point. |
SR2ARightFlag | Returns or sets the right SR2A alternative point flag. |
SR2BLeft | Returns or sets the left SR2B alternative point. |
SR2BLeftFlag | Returns or sets the left SR2B alternative point flag. |
SR2BRight | Returns or sets the right SR2B alternative point. |
SR2BRightFlag | Returns or sets the right SR2B alternative point flag. |
SR2Left | Returns or sets the left SR2 alternative point. |
SR2LeftFlag | Returns or sets the left SR2 alternative point flag. |
SR2Offset | Returns the offset used to position SR2. |
SR2Right | Returns or sets the right SR2 alternative point. |
SR2RightFlag | Returns or sets the right SR2 alternative point flag. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CreateGeometry¶
-
HeadImpactSideRailDetailBuilder.
CreateGeometry
¶ Returns or sets the create construction geometry flag.
-------------------------------------
Getter Method
Signature
CreateGeometry
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateGeometry
Parameters: createGeometry (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT11Left¶
-
HeadImpactSideRailDetailBuilder.
PT11Left
¶ Returns or sets the left PT11 additional geometry.
-------------------------------------
Getter Method
Signature
PT11Left
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT11Left
Parameters: pt11Left ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT11LeftFlag¶
-
HeadImpactSideRailDetailBuilder.
PT11LeftFlag
¶ Returns or sets the left PT11 additional geometry flag.
-------------------------------------
Getter Method
Signature
PT11LeftFlag
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT11LeftFlag
Parameters: pt11LeftFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT11Right¶
-
HeadImpactSideRailDetailBuilder.
PT11Right
¶ Returns or sets the right PT11 additional geometry.
-------------------------------------
Getter Method
Signature
PT11Right
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT11Right
Parameters: pt11Right ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT11RightFlag¶
-
HeadImpactSideRailDetailBuilder.
PT11RightFlag
¶ Returns or sets the right PT11 additional geometry flag.
-------------------------------------
Getter Method
Signature
PT11RightFlag
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT11RightFlag
Parameters: pt11RightFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT12Left¶
-
HeadImpactSideRailDetailBuilder.
PT12Left
¶ Returns or sets the left PT12 additional geometry.
-------------------------------------
Getter Method
Signature
PT12Left
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT12Left
Parameters: pt12Left ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT12LeftFlag¶
-
HeadImpactSideRailDetailBuilder.
PT12LeftFlag
¶ Returns or sets the left PT12 additional geometry flag.
-------------------------------------
Getter Method
Signature
PT12LeftFlag
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT12LeftFlag
Parameters: pt12LeftFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT12Right¶
-
HeadImpactSideRailDetailBuilder.
PT12Right
¶ Returns or sets the right PT12 additional geometry.
-------------------------------------
Getter Method
Signature
PT12Right
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT12Right
Parameters: pt12Right ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT12RightFlag¶
-
HeadImpactSideRailDetailBuilder.
PT12RightFlag
¶ Returns or sets the right PT12 additional geometry flag.
-------------------------------------
Getter Method
Signature
PT12RightFlag
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT12RightFlag
Parameters: pt12RightFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT14Left¶
-
HeadImpactSideRailDetailBuilder.
PT14Left
¶ Returns or sets the left PT14 additional geometry.
-------------------------------------
Getter Method
Signature
PT14Left
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT14Left
Parameters: pt14Left ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT14LeftFlag¶
-
HeadImpactSideRailDetailBuilder.
PT14LeftFlag
¶ Returns or sets the left PT14 additional geometry flag.
-------------------------------------
Getter Method
Signature
PT14LeftFlag
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT14LeftFlag
Parameters: pt14LeftFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT14Right¶
-
HeadImpactSideRailDetailBuilder.
PT14Right
¶ Returns or sets the right PT14 additional geometry.
-------------------------------------
Getter Method
Signature
PT14Right
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT14Right
Parameters: pt14Right ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PT14RightFlag¶
-
HeadImpactSideRailDetailBuilder.
PT14RightFlag
¶ Returns or sets the right PT14 additional geometry flag.
-------------------------------------
Getter Method
Signature
PT14RightFlag
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PT14RightFlag
Parameters: pt14RightFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ReqHorizontalLeftExact¶
-
HeadImpactSideRailDetailBuilder.
ReqHorizontalLeftExact
¶ Returns the left horizontal required approach angle.
-------------------------------------
Getter Method
Signature
ReqHorizontalLeftExact
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ReqHorizontalRightExact¶
-
HeadImpactSideRailDetailBuilder.
ReqHorizontalRightExact
¶ Returns the right horizontal required approach angle.
-------------------------------------
Getter Method
Signature
ReqHorizontalRightExact
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ReqVerticalMax¶
-
HeadImpactSideRailDetailBuilder.
ReqVerticalMax
¶ Returns the vertical maximum required approach angle.
-------------------------------------
Getter Method
Signature
ReqVerticalMax
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ReqVerticalMin¶
-
HeadImpactSideRailDetailBuilder.
ReqVerticalMin
¶ Returns the vertical minimum required approach angle.
-------------------------------------
Getter Method
Signature
ReqVerticalMin
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
SR1Left¶
-
HeadImpactSideRailDetailBuilder.
SR1Left
¶ Returns or sets the left SR1 alternative point.
-------------------------------------
Getter Method
Signature
SR1Left
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR1Left
Parameters: sr1Left ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR1LeftFlag¶
-
HeadImpactSideRailDetailBuilder.
SR1LeftFlag
¶ Returns or sets the left SR1 alternative point flag.
-------------------------------------
Getter Method
Signature
SR1LeftFlag
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR1LeftFlag
Parameters: sr1LeftFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR1Offset¶
-
HeadImpactSideRailDetailBuilder.
SR1Offset
¶ Returns the offset used to position SR1.
-------------------------------------
Getter Method
Signature
SR1Offset
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
SR1Right¶
-
HeadImpactSideRailDetailBuilder.
SR1Right
¶ Returns or sets the right SR1 alternative point.
-------------------------------------
Getter Method
Signature
SR1Right
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR1Right
Parameters: sr1Right ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR1RightFlag¶
-
HeadImpactSideRailDetailBuilder.
SR1RightFlag
¶ Returns or sets the right SR1 alternative point flag.
-------------------------------------
Getter Method
Signature
SR1RightFlag
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR1RightFlag
Parameters: sr1RightFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2ALeft¶
-
HeadImpactSideRailDetailBuilder.
SR2ALeft
¶ Returns or sets the left SR2A alternative point.
-------------------------------------
Getter Method
Signature
SR2ALeft
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2ALeft
Parameters: sr2aLeft ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2ALeftFlag¶
-
HeadImpactSideRailDetailBuilder.
SR2ALeftFlag
¶ Returns or sets the left SR2A alternative point flag.
-------------------------------------
Getter Method
Signature
SR2ALeftFlag
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2ALeftFlag
Parameters: sr2aLeftFlag (bool) – New in version NX11.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2ARight¶
-
HeadImpactSideRailDetailBuilder.
SR2ARight
¶ Returns or sets the right SR2A alternative point.
-------------------------------------
Getter Method
Signature
SR2ARight
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2ARight
Parameters: sr2aRight ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2ARightFlag¶
-
HeadImpactSideRailDetailBuilder.
SR2ARightFlag
¶ Returns or sets the right SR2A alternative point flag.
-------------------------------------
Getter Method
Signature
SR2ARightFlag
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2ARightFlag
Parameters: sr2aRightFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2BLeft¶
-
HeadImpactSideRailDetailBuilder.
SR2BLeft
¶ Returns or sets the left SR2B alternative point.
-------------------------------------
Getter Method
Signature
SR2BLeft
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2BLeft
Parameters: sr2bLeft ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2BLeftFlag¶
-
HeadImpactSideRailDetailBuilder.
SR2BLeftFlag
¶ Returns or sets the left SR2B alternative point flag.
-------------------------------------
Getter Method
Signature
SR2BLeftFlag
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2BLeftFlag
Parameters: sr2bLeftFlag (bool) – New in version NX11.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2BRight¶
-
HeadImpactSideRailDetailBuilder.
SR2BRight
¶ Returns or sets the right SR2B alternative point.
-------------------------------------
Getter Method
Signature
SR2BRight
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2BRight
Parameters: sr2bRight ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2BRightFlag¶
-
HeadImpactSideRailDetailBuilder.
SR2BRightFlag
¶ Returns or sets the right SR2B alternative point flag.
-------------------------------------
Getter Method
Signature
SR2BRightFlag
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SR2BRightFlag
Parameters: sr2bRightFlag (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SR2Left¶
-
HeadImpactSideRailDetailBuilder.
SR2Left
¶ Returns or sets the left SR2 alternative point.
-------------------------------------
Getter Method
Signature
SR2Left
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ALeft()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
SR2Left
Parameters: sr2Left ( NXOpen.Point
) –New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ALeft()
instead.License requirements: nx_general_packaging (“NX General Packaging”)
SR2LeftFlag¶
-
HeadImpactSideRailDetailBuilder.
SR2LeftFlag
¶ Returns or sets the left SR2 alternative point flag.
-------------------------------------
Getter Method
Signature
SR2LeftFlag
Returns: Return type: bool New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ALeftFlag()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
SR2LeftFlag
Parameters: sr2LeftFlag (bool) – New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ALeftFlag()
instead.License requirements: nx_general_packaging (“NX General Packaging”)
SR2Offset¶
-
HeadImpactSideRailDetailBuilder.
SR2Offset
¶ Returns the offset used to position SR2.
-------------------------------------
Getter Method
Signature
SR2Offset
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
SR2Right¶
-
HeadImpactSideRailDetailBuilder.
SR2Right
¶ Returns or sets the right SR2 alternative point.
-------------------------------------
Getter Method
Signature
SR2Right
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ARight()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
SR2Right
Parameters: sr2Right ( NXOpen.Point
) –New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ARight()
instead.License requirements: nx_general_packaging (“NX General Packaging”)
SR2RightFlag¶
-
HeadImpactSideRailDetailBuilder.
SR2RightFlag
¶ Returns or sets the right SR2 alternative point flag.
-------------------------------------
Getter Method
Signature
SR2RightFlag
Returns: Return type: bool New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ARightFlag()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
SR2RightFlag
Parameters: sr2RightFlag (bool) – New in version NX9.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Features.VehicleDesign.HeadImpactSideRailDetailBuilder.SR2ARightFlag()
instead.License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
HeadImpactSideRailDetailBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.