HeadImpactBuilderCalculationType Enumeration

NXOpen.Features.VehicleDesign.HeadImpactBuilder.CalculationType is an alias for NXOpen.Features.VehicleDesign.HeadImpactBuilderCalculationType

class NXOpen.Features.VehicleDesign.HeadImpactBuilderCalculationType

Bases: object

Represents the calculation types.

Enum Members

Enum Member Enum Member Description
BothSides
RightSide
LeftSide
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.