GroundClearanceBuilderWheelType Enumeration

NXOpen.Features.VehicleDesign.GroundClearanceBuilder.WheelType is an alias for NXOpen.Features.VehicleDesign.GroundClearanceBuilderWheelType

class NXOpen.Features.VehicleDesign.GroundClearanceBuilderWheelType

Bases: object

Represents the type of the wheel size option for ground clearance.

Enum Members

Enum Member Enum Member Description
StaticRadius
Diameter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.