GroundClearanceBuilderSurfaceLengthType Enumeration

NXOpen.Features.VehicleDesign.GroundClearanceBuilder.SurfaceLengthType is an alias for NXOpen.Features.VehicleDesign.GroundClearanceBuilderSurfaceLengthType

class NXOpen.Features.VehicleDesign.GroundClearanceBuilderSurfaceLengthType

Bases: object

Represents the type of general surface length to create ground clearace.

Enum Members

Enum Member Enum Member Description
FrontToRear
FullVehicle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.