GroundClearanceBuilderRequirementControls Enumeration

NXOpen.Features.VehicleDesign.GroundClearanceBuilder.RequirementControls is an alias for NXOpen.Features.VehicleDesign.GroundClearanceBuilderRequirementControls

class NXOpen.Features.VehicleDesign.GroundClearanceBuilderRequirementControls

Bases: object

This enum represents the standard or user defined requirement options for ground clearance.

Enum Members

Enum Member Enum Member Description
StandardDriven
UserDefined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.