GroundClearanceBuilderPositionType Enumeration

NXOpen.Features.VehicleDesign.GroundClearanceBuilder.PositionType is an alias for NXOpen.Features.VehicleDesign.GroundClearanceBuilderPositionType

class NXOpen.Features.VehicleDesign.GroundClearanceBuilderPositionType

Bases: object

Represents the ground clearance positions.

Enum Members

Enum Member Enum Member Description
Front
Rear
Both
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.