CloseRangeBlindVolumeListItemBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
CloseRangeBlindVolumeListItemBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the builder to create blind volume list item used for close range visibility.
This class is sub-object of another builder, and cannot be directly instantiated.
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
EndParameter | Returns the end parameter value on the path curve of the blind volume area. |
MaximumLength | Returns the maximum length calculated from the rear end wheel of the cylinder located to the blind volume area. |
MeasuredLength | Returns the measured length calculated from start parameter path curve point to end parameter path curve point. |
StartParameter | Returns the start parameter value on the path curve of the blind volume area. |
Status | Returns the indication if the measured length of blind volume area is acceptable or not. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EndParameter¶
-
CloseRangeBlindVolumeListItemBuilder.
EndParameter
¶ Returns the end parameter value on the path curve of the blind volume area.
-------------------------------------
Getter Method
Signature
EndParameter
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
MaximumLength¶
-
CloseRangeBlindVolumeListItemBuilder.
MaximumLength
¶ Returns the maximum length calculated from the rear end wheel of the cylinder located to the blind volume area.
-------------------------------------
Getter Method
Signature
MaximumLength
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
MeasuredLength¶
-
CloseRangeBlindVolumeListItemBuilder.
MeasuredLength
¶ Returns the measured length calculated from start parameter path curve point to end parameter path curve point.
-------------------------------------
Getter Method
Signature
MeasuredLength
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
StartParameter¶
-
CloseRangeBlindVolumeListItemBuilder.
StartParameter
¶ Returns the start parameter value on the path curve of the blind volume area.
-------------------------------------
Getter Method
Signature
StartParameter
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
CloseRangeBlindVolumeListItemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.