BumperPendulumBuilderVisualizationType Enumeration

NXOpen.Features.VehicleDesign.BumperPendulumBuilder.VisualizationType is an alias for NXOpen.Features.VehicleDesign.BumperPendulumBuilderVisualizationType

class NXOpen.Features.VehicleDesign.BumperPendulumBuilderVisualizationType

Bases: object

Represents the visualization types of the output.

Enum Members

Enum Member Enum Member Description
Curve
Surface
CurveandSurface
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.