BaseDataWheelBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
BaseDataWheelBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.VehicleDesign.BaseDataWheelBuilder
.This class can only be used in base data, thus cannot be created directly by user.
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Camber | Returns or sets the wheel camber in degree. |
CoordinateX | Returns or sets the x coordinate of right wheel center point or attachment point. |
CoordinateY | Returns or sets the y coordinate of right wheel center point or attachment point. |
CoordinateZ | Returns or sets the z coordinate of right wheel center point or attachment point. |
Diameter | Returns or sets the norminal diameter of the wheel. |
Name | Returns or sets the name of the wheel. |
PositionDefinition | Returns or sets the value to indicate which option is used to define the wheel position. |
RimOffset | Returns or sets the rim offset. |
ShowSurface | Returns or sets the option to indicate whether to show surface or not. |
ShowWireframe | Returns or sets the option to indicate whether to show curve or not. |
StaticRadius | Returns or sets the static radius of the wheel. |
Tag | Returns the Tag for this object. |
Toe | Returns or sets the wheel toe in/out in degreee. |
Track | Returns the track of the axle. |
Width | Returns or sets the width of the wheel. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BaseDataWheelBuilderPositionDefinitionOptions Enumeration | This enum represents the options to define the wheel position. |
Property Detail¶
Camber¶
-
BaseDataWheelBuilder.
Camber
¶ Returns or sets the wheel camber in degree.
-------------------------------------
Getter Method
Signature
Camber
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Camber
Parameters: dValue (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
CoordinateX¶
-
BaseDataWheelBuilder.
CoordinateX
¶ Returns or sets the x coordinate of right wheel center point or attachment point.
If
NXOpen.Features.VehicleDesign.BaseDataWheelBuilder.PositionDefinition()
isNXOpen.Features.VehicleDesign.BaseDataWheelBuilderPositionDefinitionOptions.WheelCenterPoint
, it is center point x coordinate. IfNXOpen.Features.VehicleDesign.BaseDataWheelBuilder.PositionDefinition`()
isNXOpen.Features.VehicleDesign.BaseDataWheelBuilderPositionDefinitionOptions.AttachmentPointRimOffset
, it is attachment point x coordinate. The left wheel will be located symmetrical to the vehicle centerline.-------------------------------------
Getter Method
Signature
CoordinateX
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoordinateX
Parameters: dValue (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
CoordinateY¶
-
BaseDataWheelBuilder.
CoordinateY
¶ Returns or sets the y coordinate of right wheel center point or attachment point.
If
NXOpen.Features.VehicleDesign.BaseDataWheelBuilder.PositionDefinition`()
isNXOpen.Features.VehicleDesign.BaseDataWheelBuilderPositionDefinitionOptions.WheelCenterPoint
, it is center point y coordinate. IfNXOpen.Features.VehicleDesign.BaseDataWheelBuilder.PositionDefinition`()
isNXOpen.Features.VehicleDesign.BaseDataWheelBuilderPositionDefinitionOptions.AttachmentPointRimOffset
, it is attachment point y coordinate. The left wheel will be located symmetrical to the vehicle centerline.-------------------------------------
Getter Method
Signature
CoordinateY
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoordinateY
Parameters: dValue (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
CoordinateZ¶
-
BaseDataWheelBuilder.
CoordinateZ
¶ Returns or sets the z coordinate of right wheel center point or attachment point.
If
NXOpen.Features.VehicleDesign.BaseDataWheelBuilder.PositionDefinition`()
isNXOpen.Features.VehicleDesign.BaseDataWheelBuilderPositionDefinitionOptions.WheelCenterPoint
, it is center point z coordinate. IfNXOpen.Features.VehicleDesign.BaseDataWheelBuilder.PositionDefinition`()
isNXOpen.Features.VehicleDesign.BaseDataWheelBuilderPositionDefinitionOptions.AttachmentPointRimOffset
, it is attachment point z coordinate. The left wheel will be located symmetrical to the vehicle centerline.-------------------------------------
Getter Method
Signature
CoordinateZ
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoordinateZ
Parameters: dValue (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Diameter¶
-
BaseDataWheelBuilder.
Diameter
¶ Returns or sets the norminal diameter of the wheel.
-------------------------------------
Getter Method
Signature
Diameter
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Diameter
Parameters: dValue (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Name¶
-
BaseDataWheelBuilder.
Name
¶ Returns or sets the name of the wheel.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PositionDefinition¶
-
BaseDataWheelBuilder.
PositionDefinition
¶ Returns or sets the value to indicate which option is used to define the wheel position.
-------------------------------------
Getter Method
Signature
PositionDefinition
Returns: Return type: NXOpen.Features.VehicleDesign.BaseDataWheelBuilderPositionDefinitionOptions
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PositionDefinition
Parameters: positionDefinition ( NXOpen.Features.VehicleDesign.BaseDataWheelBuilderPositionDefinitionOptions
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RimOffset¶
-
BaseDataWheelBuilder.
RimOffset
¶ Returns or sets the rim offset.
Rim offset is the shift between the mounting point of the wheel and the wheel center. It is used only when
NXOpen.Features.VehicleDesign.BaseDataWheelBuilder.PositionDefinition`()
isNXOpen.Features.VehicleDesign.BaseDataWheelBuilderPositionDefinitionOptions.AttachmentPointRimOffset
.-------------------------------------
Getter Method
Signature
RimOffset
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RimOffset
Parameters: dValue (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowSurface¶
-
BaseDataWheelBuilder.
ShowSurface
¶ Returns or sets the option to indicate whether to show surface or not.
If it is true, the wheel surface is shown.
-------------------------------------
Getter Method
Signature
ShowSurface
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowSurface
Parameters: showFace (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowWireframe¶
-
BaseDataWheelBuilder.
ShowWireframe
¶ Returns or sets the option to indicate whether to show curve or not.
If it is true, the wheel curve is shown.
-------------------------------------
Getter Method
Signature
ShowWireframe
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowWireframe
Parameters: showWire (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
StaticRadius¶
-
BaseDataWheelBuilder.
StaticRadius
¶ Returns or sets the static radius of the wheel.
-------------------------------------
Getter Method
Signature
StaticRadius
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StaticRadius
Parameters: dValue (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Toe¶
-
BaseDataWheelBuilder.
Toe
¶ Returns or sets the wheel toe in/out in degreee.
-------------------------------------
Getter Method
Signature
Toe
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Toe
Parameters: dValue (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Track¶
-
BaseDataWheelBuilder.
Track
¶ Returns the track of the axle.
Track is a computed value - the distance between the right wheel center point and the left wheel center point.
-------------------------------------
Getter Method
Signature
Track
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
Width¶
-
BaseDataWheelBuilder.
Width
¶ Returns or sets the width of the wheel.
-------------------------------------
Getter Method
Signature
Width
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width
Parameters: dValue (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
BaseDataWheelBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.