BaseDataImportExportBuilderExportOptions Enumeration

NXOpen.Features.VehicleDesign.BaseDataImportExportBuilder.ExportOptions is an alias for NXOpen.Features.VehicleDesign.BaseDataImportExportBuilderExportOptions

class NXOpen.Features.VehicleDesign.BaseDataImportExportBuilderExportOptions

Bases: object

This enum represents the option to indicate if the expressions are to be exported to a new item or an existing item in Teamcenter.

Enum Members

Enum Member Enum Member Description
NewItem
ExistingItem
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.