AllAroundVisionBuilderWindowTypes Enumeration¶
NXOpen.Features.VehicleDesign.AllAroundVisionBuilder.WindowTypes is an alias for NXOpen.Features.VehicleDesign.AllAroundVisionBuilderWindowTypes
-
class
NXOpen.Features.VehicleDesign.
AllAroundVisionBuilderWindowTypes
¶ Bases:
object
Used to indicate the type of geometry used to define the window.
Enum Members
Enum Member Enum Member Description Face Face Object for Windows. Curve Curve Object for Windows. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-