VariableOffsetBuilderMethodOptions Enumeration¶
NXOpen.Features.VariableOffsetBuilder.MethodOptions is an alias for NXOpen.Features.VariableOffsetBuilderMethodOptions
-
class
NXOpen.Features.
VariableOffsetBuilderMethodOptions
¶ Bases:
object
offset methods for creating the new surface
Enum Members
Enum Member Enum Member Description Linear linear offset applied along both of U and V directions Cubic cublic offset applied along both of U and V directions -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-