VarOffsetFaceBuilderContinuity Enumeration

NXOpen.Features.VarOffsetFaceBuilder.Continuity is an alias for NXOpen.Features.VarOffsetFaceBuilderContinuity

class NXOpen.Features.VarOffsetFaceBuilderContinuity

Bases: object

bridge continuity

Enum Members

Enum Member Enum Member Description
Connected
Tangent
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.