UserDefinedFeatureClass Class¶
-
class
NXOpen.Features.
UserDefinedFeatureClass
¶ Bases:
NXOpen.TransientObject
JA interface for UserDefinedFeatureClass
An instance of this class can be obtained from
Features.UserDefinedFeatureClassManager.CreateClass()
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
AddCopyHandler | Registers the copy callback. |
AddCreateHandler | Registers the create callback. |
AddEditHandler | Registers the edit callback. |
AddIconHandler | Registers the udf icon callback. |
AddUpdateHandler | Registers the udf update callback. |
Dispose | Frees the memory associated with this object. |
Property Detail¶
Method Detail¶
AddCopyHandler¶
-
UserDefinedFeatureClass.
AddCopyHandler
¶ Registers the copy callback.
Signature
AddCopyHandler(copyCallback)
Parameters: copyCallback (CallableObject) – New in version NX8.0.0.
License requirements: None.
AddCreateHandler¶
-
UserDefinedFeatureClass.
AddCreateHandler
¶ Registers the create callback.
Signature
AddCreateHandler(createCallback)
Parameters: createCallback (CallableObject) – New in version NX8.0.0.
License requirements: None.
AddEditHandler¶
-
UserDefinedFeatureClass.
AddEditHandler
¶ Registers the edit callback.
Signature
AddEditHandler(editCallback)
Parameters: editCallback (CallableObject) – New in version NX8.0.0.
License requirements: None.
AddIconHandler¶
-
UserDefinedFeatureClass.
AddIconHandler
¶ Registers the udf icon callback.
Signature
AddIconHandler(iconCallback)
Parameters: iconCallback (CallableObject) – New in version NX8.0.0.
License requirements: None.