TrimCurveBuilderFirstBoundingObjectEndOptions Enumeration¶
NXOpen.Features.TrimCurveBuilder.FirstBoundingObjectEndOptions is an alias for NXOpen.Features.TrimCurveBuilderFirstBoundingObjectEndOptions
-
class
NXOpen.Features.
TrimCurveBuilderFirstBoundingObjectEndOptions
¶ Bases:
object
Represents the trim curve first bounding object end options
Enum Members
Enum Member Enum Member Description Start Trim first bounding object from start End Trim first bounding object from end -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-