ThroughCurvesBuilderConstructionMethod Enumeration¶
NXOpen.Features.ThroughCurvesBuilder.ConstructionMethod is an alias for NXOpen.Features.ThroughCurvesBuilderConstructionMethod
-
class
NXOpen.Features.
ThroughCurvesBuilderConstructionMethod
¶ Bases:
object
This enum represents the Construction options.
Enum Members
Enum Member Enum Member Description Normal Use the standard procedures. SplinePoints Use the points and tangent values at the points for reparameterizing curves. Simple Build the simplest mesh surface possible. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-