ThroughCurveMeshBuilderEmphasisType Enumeration¶
NXOpen.Features.ThroughCurveMeshBuilder.EmphasisType is an alias for NXOpen.Features.ThroughCurveMeshBuilderEmphasisType
-
class
NXOpen.Features.
ThroughCurveMeshBuilderEmphasisType
¶ Bases:
object
This enum represents the Emphasis options.
Enum Members
Enum Member Enum Member Description Both Emphasis on both primary and cross strings. Primary Emphasis on primary strings. Cross Emphasis on cross strings. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-