TabNoteCfgBuilder Class¶
-
class
NXOpen.Features.
TabNoteCfgBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Features.TabNoteCfgBuilder
New in version NX5.0.3.
Properties¶
Property | Description |
---|---|
BlockOffset | Returns or sets the block offset |
DeletePreviousDiagrams | Returns or sets the delete previous diagrams |
InsertionPoint | Returns or sets the insertion point |
NumberOfRows | Returns or sets the number of rows |
ReferencePlane | Returns or sets the reference plane |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TabNoteCfgBuilderRefplane Enumeration | the reference plane type. |
Property Detail¶
BlockOffset¶
-
TabNoteCfgBuilder.
BlockOffset
¶ Returns or sets the block offset
-------------------------------------
Getter Method
Signature
BlockOffset
Returns: Return type: float New in version NX5.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlockOffset
Parameters: blockOffset (float) – New in version NX5.0.3.
License requirements: nx_ship_concept (“Ship Concept”)
DeletePreviousDiagrams¶
-
TabNoteCfgBuilder.
DeletePreviousDiagrams
¶ Returns or sets the delete previous diagrams
-------------------------------------
Getter Method
Signature
DeletePreviousDiagrams
Returns: Return type: bool New in version NX5.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeletePreviousDiagrams
Parameters: deletePreviousDiagrams (bool) – New in version NX5.0.3.
License requirements: nx_ship_concept (“Ship Concept”)
InsertionPoint¶
-
TabNoteCfgBuilder.
InsertionPoint
¶ Returns or sets the insertion point
-------------------------------------
Getter Method
Signature
InsertionPoint
Returns: Return type: NXOpen.Point
New in version NX5.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
InsertionPoint
Parameters: insertionPoint ( NXOpen.Point
) –New in version NX5.0.3.
License requirements: nx_ship_concept (“Ship Concept”)
NumberOfRows¶
-
TabNoteCfgBuilder.
NumberOfRows
¶ Returns or sets the number of rows
-------------------------------------
Getter Method
Signature
NumberOfRows
Returns: Return type: int New in version NX5.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfRows
Parameters: numberOfRows (int) – New in version NX5.0.3.
License requirements: nx_ship_concept (“Ship Concept”)
ReferencePlane¶
-
TabNoteCfgBuilder.
ReferencePlane
¶ Returns or sets the reference plane
-------------------------------------
Getter Method
Signature
ReferencePlane
Returns: Return type: NXOpen.Features.TabNoteCfgBuilderRefplane
New in version NX5.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferencePlane
Parameters: referencePlane ( NXOpen.Features.TabNoteCfgBuilderRefplane
) –New in version NX5.0.3.
License requirements: nx_ship_concept (“Ship Concept”)
Method Detail¶
Validate¶
-
TabNoteCfgBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.