SweptBuilderSectionLocationTypes Enumeration¶
NXOpen.Features.SweptBuilder.SectionLocationTypes is an alias for NXOpen.Features.SweptBuilderSectionLocationTypes
-
class
NXOpen.Features.
SweptBuilderSectionLocationTypes
¶ Bases:
object
This enum represents the Section Location option. If a single section located at the middle of a guide string is specified, Anywhere Along Guides option sweeps in both directions.
Enum Members
Enum Member Enum Member Description AnywhereAlongGuides Anywhere along Guides EndsOfGuides Ends of Guides -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-